Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide22

Any rapid rise in temperature will open the thermal link which will permanently disconnect the MOV from the circuit. Thermal runaway, with all of its dangers, is eliminated by this action and is no longer a threat. When the thermal fuse opens, current will instantly fall to zero and the temperature will begin to decrease as shown in the graph. Once the thermal fuse opens, it will never close again and reestablish current flow. The TMOV is a one-time-acting device similar to a conventional overcurrent fuse.

PTM פורסם ב: