Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide5

Nearby lightning strikes will cause a fast moving electromagnetic wave to radiate out in all directions. There can be huge amounts of energy coupled into any wires that lie in its path. This will happen regardless if the wires are overhead on telephone poles or buried underground. A lightning strike one mile away will produce a 70V transient on overhead wires; if the strike is only 500 feet away, the transient will reach 10,000V. Any item connected to these wires will need protection from the overvoltage event to prevent certain damage.

PTM פורסם ב: