Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide3

MOV is the abbreviation for Metal Oxide Varistor, sometimes referred to as a Varistor or VDR. An MOV is a type of device in which the resistance changes depending upon the applied voltage. The electrical operation of the device is similar to that of two zener diodes placed in an anode-to-anode configuration. Because of this electrical behavior, they can be used to absorb excess energy initiated by an overvoltage event and thereby protect downstream circuit components from damage.

PTM פורסם ב: