Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide50

In summary, Metal Oxide Varistors are high energy devices designed to protect against overvoltage events. They are normally found protecting the AC line feeding an item. Smaller types, frequently referred to as Varistors, protect circuitry deeper inside an application at the PC board level. Thermally protected TMOVs, which disconnect the power source when an MOV fails offer the designer a way to lessen the chances of catastrophic damage. The TMOV is also available in an iTMOV style which features a third lead from the MOV/fuse junction for monitoring. A wide variety of sizes and mounting styles, from surface mount devices and radial leaded MOVs to screw terminal industrial MOVs, are offered to accommodate a wide assortment of applications. Factors to consider when selecting an MOV for an application are; the continuous voltage rating, the physical size of the device, the energy and peak current rating, maximum clamping voltage and the Varistor voltage. It should be remembered that the continuous voltage rating should be 10% to 20% higher than the maximum circuit voltage. The physical size of the MOV depends on the transient energy or current expected, or the required clamping voltage. Finally, the MLN Surge Array™ offers a 1206 package surface mount device containing four MLVs. Available in 5.5V, 9V, 14V and 18V ratings, the MLN has an inherent capacitance that can provide additional filtering to the DC line. The 1206 package also offers considerable PC board space savings over individual MOVs.

PTM פורסם ב: