Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide13

This slide shows how temperature affects an MOV. As can be seen, most of the change in the current occurs at the low “leakage” end of the V/I curve. As the current increases, the dependence upon temperature is much less pronounced and is usually neglected up to the maximum temperature allowed for a particular MOV family. All of the available datasheets contain derating information for operation at elevated temperatures. Keep in mind that an MOV is not intended for voltage regulation where there is a continuous DC current flow. MOVs are designed to protect downstream circuitry from the occasional overvoltage transient event which lasts no more than a millisecond or two. The average continuous power that can be handled by an MOV is normally less than 1W, but the transient power is thousands of Watts.

PTM פורסם ב: