Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide25

Here a Gas Discharge Tube that has been added in series with the MOV going from the hot line to ground. Many consumer products have a grounded metal cabinet which can become a shock hazard if the MOV leakage current becomes high. This problem is completely solved by the GDT which will electrically disconnect the MOV from ground while the GDT is not conducting. Any potential leakage current from the MOV is thereby prevented and the shock hazard is eliminated. During a high voltage transient above the GDT threshold, it will instantly begin conducting and reestablish the MOV connection to ground.

PTM פורסם ב: