Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide15

These are definitions that need to be understood before an MOV selection can be made; and most are self explanatory. The first point, though, may appear to be incorrect, but it is true that the continuous voltage rating should be 10% to 20% higher than the maximum circuit voltage encountered. UL has chosen a 15% factor and calls it the MCOV, or Maximum Continuous Operating Voltage. Following this selection criteria will ensure enough operating margin to keep leakage currents from exceeding the MOV conduction point. For example, on a 120VAC line, a 150V MOV should be selected. Some users do not follow this guideline, but it should be adhered to in order to avoid premature MOV failure.

PTM פורסם ב: