Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Product List
MOV-Slide20

The TMOV™ is constructed with a conventional MOV ceramic disc and a thermal cutoff device inside the same housing. Sometimes a conventional MOV will be exposed to an energy level that is beyond its capabilities. Or sometimes an MOV has reached the end of its useful life and just shorts out. Either of these conditions can result in rapid burning or fragmentation. It is important to disconnect the MOV from the circuit as quickly as possible to lessen the chance of serious damage. TMOV response time is ultra fast because the thermal cutoff component is mounted inside the part on the ceramic disc itself. This is still not a 100% solution to MOV destruction, however. There is always the possibility of a very large transient coming in that can destroy even a TMOV. This is just another level of insurance against the possibility of physical damage.

PTM פורסם ב: