Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Slide10

The installation dimension of 9.2 mm must be observed when assembling the RAFIX FS front panel and PCB. Suitable spacers are available from the accessories range. The length is calculated using the following formula: 9.2 mm minus the front panel thickness equals the length of the spacer.

PTM פורסם ב: