Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Slide14
The actuators from the RAFIX 22 FS+ series offer at least an IP65 degree of protection. This means that they can be used in various applications. The mechanical operating life of all actuators is ideally suited for longstanding use, even in heavily used panels.
PTM פורסם ב: