Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Slide2

The RAFIX 22 FS+ series is the benchmark in the field of control components. The extremely flat style and the functional yet aesthetic design are indispensable in an increasingly design-oriented industrial environment. The large selection and variability of the actuating elements gives the designer all kinds of creative freedom: Round or square collar shapes, bright colors with the homogeneous illumination of the large actuating area are the foundations for this. The combination with the various front rings ensures that the designer’s panel boasts an individual recognition factor. For instance, a defined color can always be assigned to a certain input command. Not only that, the numerous front ring color options allowed the user to customize the system to the corporate design of the respective OEM.

PTM פורסם ב: