Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
MOSFET-Slide3

ROHM’s ECOMOS™ series of MOSFETs has features that include low voltage operation from 1.2V along with compact, low profile, high power packages. Another major feature of these devices is their low RDS(on). As can be seen in the plot here, this lower RDS(on) results in an approximate 90% drop in power consumption while in the ON state when compared to conventional 2.5V MOSFETs. Additionally, the ECOMOS™ Series is available in a number of different packages in order to suit various application needs.

PTM פורסם ב: