Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 16
When using capacitive sensing for touch applications the PCB trace typically acts as one plate of the capacitor. When a conductive object, such as a finger for touch sensing, comes into proximity it acts as the other plate and the air is the dielectric. As the object moves closer to the pad the capacitance changes, based on the equation for capacitance shown in this slide. The constants in the equation represent the value for the dielectric constant of the material, i.e. air, glass etc. The value for the term “A” is a measure of the area of the pad used for the sensor capacitor and the term “d” represents the distance between the two plates. Therefore, for touch applications, as the finger moves closer to a pad, the value for “d” is reduced which increases the capacitance.
PTM פורסם ב: