Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 23
In earlier versions of the capacitive sensing module the auto-scan feature converted all of the channels between the start channel and the ending channel. This was not necessarily the most efficient method for scanning several channels. In the CS0 module, the channels that are included in the scan are enabled by setting mask bits. Only the channels with a mask bit set to ‘1’ are used to set the CS0 mux bits. Only including the channels that are required to be converted in the auto-scan sequence greatly reduces power since only the necessary channels are being converted (i.e. reduced number of conversions).
PTM פורסם ב: