Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 28
The simplest implementation of capacitive sensing is the single touch, where simple threshold techniques can be used to generate the feedback for the API to perform the required functions.  For example, only the Inactive to Active and Active to Inactive thresholds are used to determine when the rising-edge event and falling-edge event callback functions are used in the API. A single element of a slider can also be used as single touch which may be useful to start a scan of larger human interface sensors such as sliders.
PTM פורסם ב: