Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 34
The Silicon Labs F990SliderEK evaluation kit is a great low power application example to start the user in developing a touch slider solution. The EK does not feature an OFF switch, further testament to the low-power nature of the F990. With a coin cell battery on the back-side and LEDs along the capacitive touch area – the EK layout provides an example of good layout guidelines and, more importantly, great low-power design considerations. This self-contained demonstration unit also comes with schematics, layout drawings, and example code.
PTM פורסם ב: