Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 9
The wake-up time of the MCU is a very important aspect of low power system design. The wake-up time is the amount of time it takes the MCU to start executing instructions from the low power mode and is dependent on which mode the MCU is exiting. Another extremely important aspect of low power systems relating to wake-up time is the analog settling time requirement.  Many applications wake-up and take an ADC reading and go back into sleep mode so it is not sufficient to just look at the digital wake-up time anymore. The analog system needs to be up and ready to take a measurement quickly so the MCU can return to the low power state.
PTM פורסם ב: