Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 39
In battery meter mode, the system measures the battery voltage and slowly blinks an LED to indicate the approximate battery life remaining. If the MAX LED is blinking, then the battery is fully charged. If the MIN LED is blinking, then the battery is nearly depleted and it is time to replace the battery. From the slider demo mode, the system will enter battery meter mode when the slider is pinched once. After entering battery meter mode, the system will remain in this mode for approximately ten seconds. The system may be held in battery meter mode for longer than ten seconds by touching the slider. The system will remain in battery meter mode as long as the slider is touched. Upon exit from battery meter mode, the system goes back into slider demo mode.
PTM פורסם ב: