Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 36
The C8051F990 Slider Evaluation Board is ready to use out of the box. Simply lay the board on a flat surface, remove the paper tab to allow the battery to make contact with the battery holder, touch the A button on the left side of the slider, and slowly slide your finger towards the B button on the right side of the slider. Once the system turns on, the two LEDs corresponding to “Mode 0: Slider Demo” will flash four times indicating that the system is in slider demo mode.
PTM פורסם ב: