Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Product List
QuickSense C8051F990 Low Power MCU with Capacitive Sensing Slide 31
It has been shown that the C8051F99x family is a low power solution that adds robust capacitive sensing. Shown here is an example of being able to implement a ‘wake on slider’ while maintaining the low power sleep modes, taking advantage of both features. In this example the system can wake-up and detect the slider motion.  Each of the channels are implemented as a set of two bonded channels creating a total of three pads that get sampled.  For clarity, the arrangement of the channels is indicated by the color differences in the diagram. The first set of pads are monitored for the start of the slider motion and the next set of pads is implemented as a group of pads for course slider motion. When the MCU has detected the wake event, the slider can be implemented using the standard algorithms.
PTM פורסם ב: