Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide11

Shown on this slide is a Bodi plot, covering the frequency range of DC to 10GHz, comparing frequency response and frequency versus impedance plots. The red trace is a passive probe, can be seen to have a very steep roll off at the higher frequencies. The blue and dark blue traces are active probe technologies which do not decrease in impedance as fast as the passive probe. This shows that passive probes provide the highest impedance below 20KHz while the transistors are good at high frequencies, with good input resistance and circuit loading.

PTM פורסם ב: