Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide27

The most desirable method is a true differential probe. As can be seen on this slide, one input channel of the oscilloscope is used. In this example the gate to the drain of the FET is being probed safely. This method has good common mode range, good common mode rejection ratio, and it is a true balanced probing technique. Also, the lead parasitic capacitance is cancelled out. All of the problems associated with floating the oscilloscope are overcome by using the proper differential signal conditioner. The oscilloscope remains safely grounded. Ground is not part of the measurement inputs.

PTM פורסם ב: