Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide17

There are also some other accessories that help probe in difficult areas. The bent sharp tip allows the user to reach inside a via when a traditional straight tip is not capable. Also the short ground lead with a spring hook or the solder-in ground can be used to reach the ground point. Remember, it is still necessary to keep the grounds as short as possible.

PTM פורסם ב: