Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide36

There are three basic methods to make current measurements: shunts, transformers and Hall Effect devices. The next three slides give more details on each of these methods. Shunts can measure DC and AC currents up to reasonably high frequency. You can break a circuit to install a shunt (as shown on the next slide) or you can embed a shunt as a sensor in the circuit. Transformers can measure AC currents (but not DC). There are inexpensive AC current probes which incorporate transformers and measure only AC current. Hall effect devices are good for measuring DC current and can also measure low frequency AC. There are trade-offs for using each of the three techniques. The best types of general purpose current probes for use with oscilloscopes combine the use of transformers and Hall effect. They can detect DC current and have flat bandwidth response for detecting currents out to fairly high frequencies (up to 100MHz).

PTM פורסם ב: