Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide2

There are four basic types of probes; passive, active, differential, and current measuring. Passive probes are standard with scopes and contain no active devices, only passive. They are physically and electrically robust and can handle very high voltage typically. Passive probes are very rugged mechanically, but the bandwidth is limited typically to 500MHz. Using a 500MHz probe at 1GHz, will create problems. Active probes are optional, they are based on transistor devices and are powered by the oscilloscope. They are not as robust as the passive probes, but are able to achieve much wider bandwidths and have much lower capacitance, typically less than 1pF. They are ideal for probing high frequencies.

PTM פורסם ב: