Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide26

Another technique is isolators, which can be transformer or optical. There are limitations such as imbalanced inputs, there is the concern of parasitic capacitance and very low common mode rejection ratio at high frequencies. An isolator is an accessory which allows oscilloscopes to safely make floating measurements. It consists of a conventional single ended oscilloscope front end (attenuator and preamplifier) protected with insulation which drives an isolation system based on either optical, transformer, or a combination of both systems. The output is a ground referenced amplifier that can connect to any oscilloscope, which remains safely grounded. The input probe is similar to a conventional attenuating scope probe, with better insulation in the ground lead to accommodate the higher reference voltages. Notice that there is no resistive path between ground and either input. There is still a capacitive element however, which will resonate with the inductance in the ground lead similar to a floating scope. This capacitance is much lower than that of the floating scope, so the effect is not as great.

PTM פורסם ב: