Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide3

Differential probes are active devices in some cases and passive in others. They are based on an amplifier with a positive and negative input. The active differential probes are transistor based. Differential probes are useful for measuring signals when there is no ground reference, for example PCI express is a differential data path which would benefit from the use of differential probes. There are also high voltage differential probes that are typically passive type devices that are able to handle very high voltages. The final type of probe is the current probe. There are three main types of current probes: transformer based, Hall Effect device based, or a combination of both transformer and Hall effect device. The majority of current probes are clamp type devices, and most of them are Hall Effect.

PTM פורסם ב: