Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide21

All of these situations, including measurements which are not referenced to ground, either require or are enhanced by a differential measurement technique. There are several ways to allow a single ended scope to make differential measurements. One method which is very common is to float the scope, this is a bad choice and should not be attempted. Other methods are to use two single ended probes and then do the math, isolators can be used, or use true differential probes.

PTM פורסם ב: