Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Product List
Fundamental-Slide28

Putting the differential amplifier into the circuit being measured, one can see how all of the problems with the single ended scope measurement are eliminated. Notice that both input leads present the same high impedance load to the circuit under test, referred to as being balanced. A good test to see if an unbalanced technique is affecting the measurement is to reverse the input leads. (Do not do this with a floating scope on circuits sensitive to excess loading capacitance.) Ideally, the waveform should be a identical but inverted. If any change in the waveform is noticeable when the input leads are reversed (use the invert function of the scope if necessary), then the circuit is susceptible to the effects of unbalanced loading.

PTM פורסם ב: