Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 20

The USCI is also configurable as an SPI port. It is also compatible with the previous generation and has a migration guide for older 2xx devices. The enhancements to the SPI mode include operation of up to 10 Mb/s maximum bit rate with a goal of reaching up to 10 MHz in the near future. There is also a modified 4 pin mode that can be used as a true chip select in master mode for easier bus communication in system.

PTM פורסם ב: