Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 22

The analog to digital converter on this new family has also been improved. It is much lower power than the previous version, about 10x lower than the ADC10 on the MSP430F2xx family. The speed remains the same at up to 200 KSPS. The device also supports its own unique reference voltage, selectable at 1.5, 2 or 2.5 volts. Similar to previous versions, it has 14 channels, two of which, however, are only usable internally for battery voltage monitoring and temperature sensing. In this new version, the Direct Transfer Controller (DTC) that was used to send read values directly to memory has been replaced by the DMA; this is much more flexible and can send the values to more places on the device to support quick operation without CPU intervention. One of the other major improvements has been the inclusion of the window comparator into the A/D. This allows the user to set different high, low, and middle thresholds to generate interrupts.

PTM פורסם ב: