Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 9

So what does this mean? Recall the evolution of Flash and its capabilities in its early days. One example is that in designing for low and ultra low power operation, memory access speeds would be restricted (to say 8 MHz) via the surrounding memory controller/power management circuitry. This reduces the power consumption of the memory IP. Typically, for most applications, system speeds can be 2 – 3x higher than the memory access speeds before memory access becomes a bottleneck. But even this can be alleviated via, for example, a small, integrated SRAM cache in the product. This approach could balance the need for performance and ultra low power memory access operation. The second major limitation is memory density and size. FRAM today is ideally suited for devices needing less than 128/256 KB of embedded memory. While TI has successfully demonstrated manufacturability of up to 4 Mbytes FRAM, the FRAM on MSP430 devices only contains up to 16kB of data on this first series of devices, the MSP430FR57xx family. Plans are in place to improve both the speed and size of FRAM in the coming years.

PTM פורסם ב: