Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 27

Finally, the section of the CPU that manages this activity in real time is the FRAM controller. This is also where the cache lives and the wait states are managed for devices that operate at over 8 MHz. Note that the cache is totally transparent to the user and operates seamlessly in execution.

PTM פורסם ב: