Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 30

There is one drawback to building products with the first generation MSP430FR57xx, and that is that it cannot be programmed and then sent through reflow or soldering. The high temperature of 260°C for about 2 minutes would cause a small number of bits to become unreliable due thermal characteristics eroding the polar margin in the FRAM molecules. This is also known as “thermal depolarization” and is not allowable in many applications where FRAM would be used as both readable and writeable memory. Any activity where these types of temperatures occur after programming should be avoided. Programming can easily be completed by in circuit testers, flying probes, production board level programmers, and even serial bootstrap loader interfaces. In addition, there are many other ways to program these devices after they have been soldered onto the board. There is no problem with this method, as successfully writing the memory even once after the soldering will reset the memory to behave like the thermal exposure never happened. Finally, this behavior has been resolved in future generations of MSP430 FRAM parts after the initial MSP430FR57xx family. Reflow soldering should not be a problem for devices released in 2012 and beyond.

PTM פורסם ב: