Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 8

One more area where FRAM outshines other memory types is in its write endurance. Because FRAM storage occurs in the state of a dipolar crystal instead of depending on the destructive penetration of electrons into a dielectric, it can last far longer, over 1 billion times longer in fact. This test was done with the same 512 byte sector with both memories writing constantly at 12 kilobytes per second. As one can see, the Flash memory started failing in just under 7 minutes while the FRAM could last over 100,000 years. It is useful to note that although FRAM requires a refresh when read (just like DRAM), the memory will not wear out.

PTM פורסם ב: