Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
MSP430FR57xx FRAM Microcontrollers Slide 31

Here are the features of the first family of MSP430 FRAM devices. There are 20 parts that will be included in the first release. The MSP430FR5739 is readily available for sampling and development today. The packages range from a tiny 4x4 QFN to a 38-pin TSSOP with a couple of options in between. Up to 33 I/Os are supported as well as 16 channels of ADC.

PTM פורסם ב: