Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Cyclone3-Slide11

Giga-Multiplies/s is the theoretical maximum number of 16 by 16 multiply operations that can be done in a second if all multipliers were used at full bandwidth on the DSP device or the FPGA. Cyclone® III devices have up to 288 multipliers that operate in parallel at up to 260MHz. In practical applications, these utilization levels will not be reached or required with the DSP devices or the FPGA. What this data shows is that even low-cost FPGAs now have a great deal of DSP horsepower. Because of this, FPGAs offer benefits in applications requiring a lot of parallel multiplication operations, such as a multi-channel applications including video surveillance systems, communications systems, and other spaces. Cyclone® III devices can be used to complement DSP processing deficiencies or even replace 1 or more DSP processors entirely. The net benefit is to improve system performance, lower system cost, reduce system board space, and/lower system thermal power dissipation.

PTM פורסם ב: