Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Cyclone3-Slide15

Using the remote system upgrade feature allows connection of a Cyclone® III device to a serial or parallel flash configuration device. The configuration device can be loaded with a factory image and one or more application images. At power up the known good factory image is loaded and the part goes into user mode. At some time in the future the users application can detect a new application image and trigger the device to reconfigure. If the configuration finishes without error the device goes into user mode again with the new image. If there is a problem during this process, the controller will automatically revert back to loading the known good factory image so there is zero down time.

PTM פורסם ב: