Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Cyclone3-Slide36

To summarize the Cyclone® III clocking and PLL advantages over the Cyclone® II: the outputs per PLL are increased from 3-5 to gain 8 additional PLL generated clocks, the total number of clocks was increased from 8-16 to 10-20 clocks per device, and the operating frequency was extended on the lower end to support low-cost clocks and on the higher end for higher performance devices. Additionally, the PLLs can be dynamically configured with values stored in the M9K blocks, and can be cascaded to save I/Os and ease PCB routing by eliminating the need to bring the clock off the chip and back to the device. The Cyclone® III also enables an auto-calibration feature on DDR interfaces for higher performance and an easier timing closure process.

PTM פורסם ב: