Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Cyclone3-Slide14

Every Cyclone® III device has 8 banks of I/O that can support most I/O standards, but need to be powered from 1.2V to 3.3V. Intel® recently added RSDS, Mini-LVDS and PPDS I/O compatibility to support the display market. Cyclone® III devices also support DDR2 up to 200MHz, which allows 400Mbps DDR2 interfaces on a low cost FPGA. These memory interfaces are designed using the TimeQuest timing analyzer which allows the memory interface to compensate dynamically for process, voltage and temperature changes in the system.

PTM פורסם ב: