Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Cyclone3-Slide20

A key attribute in the design of the Cyclone® III devices is its low power consumption. The design process of the Cyclone® III focused first on the silicon process used. Using TSMC’s low power 65nm process offered a huge return in lowering power consumption. This is the first time Intel has designed a family using TSMC’s low-power process, which was chosen because of its proven performance in leading cellular phone manufacturer’s designs. Using multiple transistor threshold voltages provides the opportunity to use higher threshold voltages for non-critical transistors to reduce leakage current. At times the choice was made to use a lower transistor threshold voltage for higher performance, but increased the channel length to reduce leakage current. Using a thicker gate oxide for non-critical speed transistors lowers the performance of the transistors but also reduces the leakage current flow.

PTM פורסם ב: