Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Cyclone3-Slide12

The larger memory blocks enable: performance enhancements by reducing the need to cascade memory blocks, higher memory to logic ratios allowing users to select a smaller and lower cost device for memory intensive applications such as packet processing or processor code storage, and better memory to multiplier ratio for video line buffers and to support DSP intensive applications such as general video and image processing. Memory bandwidth is defined as Memory Blocks x ports (2 per) x width of ports (36b) x Frequency (260MHz). If the Cyclone® III is compared with the Cyclone® II: the Cyclone® III’s blocks are increased, frequency has increased, and port width is the same, leading to a significant increase in memory bandwidth.

PTM פורסם ב: