Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Product List
Slide35

The ISL85033 can be designed to power any point-of-load application that requires a low to mid output voltage and high load current. In the residential market such as home automation, electronic control systems requiring high current are used in applications such as heating and gas. Other electronics in the home include electronic window blinds and door openers. In commercial markets such as office buildings, the ISL85033 could be designed to power multiple point-of-loads from a central location for AC and thermal systems, lighting control, and various forms of security. In factories that implement assembly line control and system test, multiple ISL85033 regulators could be easily designed to power the various control systems in this manufacturing environment. Other applications include test equipment and thermal chambers. Also, because of the compact size and high current capability, the ISL85033 could be designed into in a variety of applications including power tools, office printers and other offline power applications.

PTM פורסם ב: