Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
Clock and Data Distribution Products Part 2 Slide 11

This slide shows an example of how an Equalizer device can be used. The 6.25 Gbps signal goes through 15 inches of FR4 backplane and the first reading is taken right after the backplane which is shown in the left image. Then the signal traverses the 7V219M Equalizer and another reading is taken at the output of the equalizer device which is shown on the right image. It is obvious that the eye diagram is much clearer and wider after the equalizer device than before.

PTM פורסם ב: