Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
Clock and Data Distribution Products Part 2 Slide 8

Zero Delay Buffers are a special type of fanout buffers. Zero delay buffers generate multiple copies of an input clock with the phase of the output clocks aligned to the phase of the input clock giving the impression of zero delay. This is achieved by looping back one of the outputs to the feedback input of the device. Typically, any of the outputs can be used as the feedback. If a divided output is used as the feedback, what would happen to the frequency of the non-divided outputs? Their frequency would be equal to the divide ratio times the input frequency, so a divide by 2 would yield a multiplied by two non-divided output.

PTM פורסם ב: