Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
Clock and Data Distribution Products Part 2 Slide 7

This slide will take a look at generic fanout out buffers. These devices are used to generate multiple copies of an input clock. Typically they do not integrate a PLL. Fanout buffers can have multiple inputs. Some fanout buffers can support an external XTAL as input. Fanout buffers can have anywhere from 2 to 24 outputs. The acceptable input and output levels; are device dependent, but generally, all common levels are supported. The NB3N853531E depicted below has 2 inputs. One must be a single ended clock signal. The other one can only be used with an external XTAL. It is not mandatory to use both inputs. If both inputs are used the CLK_SEL (Clock Select) pin is used to choose the input clock to distribute to the outputs. As seen on this slide, the NB3N853531E has 4 differential outputs.

PTM פורסם ב: