Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
Clock and Data Distribution Products Part 2 Slide 30

This slide gives an example of a handheld device, such as a cellular phone, GPS, tablet, or any other handheld device. Typically these devices require two or more expensive TCXOs. For instance, they may need one TCXO for the GPS module and another one for the WLAN module. Using the NB3RL02, a low cost fanout buffer with one input and two outputs, and an integrated LDO is an innovative, power efficient, cost sensitive way to reduce the BOM cost of any handheld device. Only one TCXO is required instead of two. The NB3RL02 is in shutdown mode until it receives a request from either module. Once a request is received, it powers up its internal LDO and the TCXO which was previously turned. Then it sends a clock signal to the input of the NB3RL02 which finally provides the clocks to run the external modules. When both modules are turned off, the NB3RL02 goes back into shutdown mode, switching off the internal LDO which in turn shuts down the external TCXO.

PTM פורסם ב: