Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 12
There are two devices currently for IR proximity detection: the Si1102 and the Si1120. The features for each are listed in the table. The key difference is that the Si1120 provides ambient light detection and provides a PWM output directly proportional to the reflected energy. The Si1102 does not include an ALS photodiode and is used as a standalone device to provide simple binary logic detection without ambient light detection. The Si1120 ALS photodiode helps identify the background ambient light characteristics for an improved infrared result. Each of these sensors can be used in a wide variety of applications as shown in the figure.
PTM פורסם ב: