Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 25
Once the initialization sequence is completed, the firmware has to be set up to service the operation of the Si1120 using the PCA interrupt service routines (ISR). PCA channel one was configured to be the square wave output which was generated by adding the DIVIDE_RATIO value to the current count to always provide the same overflow rate. Within the channel one ISR, the next count value is determined and loaded into the compare registers to provide the next overflow. That is all the ISR does for this PCA output driving the STX signal.
PTM פורסם ב: