Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Product List
Si1102 and Si1120 Slide 4
The electromagnetic spectrum is a continuum of all electromagnetic waves arranged according to frequency and wavelength. The sun, earth, and other bodies radiate electromagnetic energy of varying wavelengths. The electromagnetic spectrum is familiar in day to day life. The microwave ovens and cell phones emit and receive energy that is part of the Electromagnetic Spectrum. The light that human eyes can see is also part of the electromagnetic spectrum. This visible part of the electromagnetic spectrum consists of the colors that are seen in a rainbow - from reds and oranges, through blues and purples. Infrared light lies between the visible and microwave portions of the electromagnetic spectrum. Infrared light has a range of wavelengths, just like visible light has wavelengths that range from red light to violet. "Near infrared" light is closest in wavelength to visible light and is what is used as the energy source in proximity sensing applications.
PTM פורסם ב: